Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the example in hand we will initially perform a Full-text search. This is opened and activated at program start by default.
The Full-text search is performed with the following settings:
Current selection (ISO) [select "Norm" -> "ISO" at the Catalogs tabbed page]
Full-text search with the following term:
hexagon bolt D=10 L=50
Detailed
information on syntax is found under Section 3.1.6.4.2, “
Full-text search
”
or directly out of the application by clicking .
-> The
view changes at the CloudNavigator
tabbed page. The graph shows concrete single parts. You can recognize
this at the respective icon
. When you move the mouse over a result, then a
tooltip
appears. There you can see the characteristic M10x50, which
exactly meets the condition.
In the next step on a result part a GeoSearch shall be performed.
Open the context menu at the desired part and click on Geometric Search.
Result: The search part of the GeoSearch moves into the center of the graph and the result parts are grouped around the search part.
The results of the first search (here Text Search) and second search (here GeoSearch) can be compared side by side. With pressed mouse button you can move the graph as a whole or single nodes. At each node you can find the context menu command Zoom, wherewith you can move the desired node into the center.
Now two hits shall be loaded into the Part comparison.
At the Cloud Navigation Search you reach the part comparison via context menu -> Common context -> Part comparison.
Once select Load as first part
and once
Load as second part.
-> The Part comparison dialog box is docked and the desired parts are transferred.
You can find detailed information on the part comparison under Section 3.1.6.10, “ Part comparison ”.