Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Follow the steps listed below to send a CAD model to your e-mail address:
In the dialog area for the download of CAD models, under Edit CAD formats -> Add CAD formats, select the transfer mode email. Then determine one or several formats and click on . (For details please see Section 4.8.2.1, “How can I select a CAD format? | How can I define the transfer mode into the CAD system? (Supplier portals)”.)
-> The view returns to the dialog area Generation options / Selected formats. Confirm your entries by clicking on .
In the dialog area for the CAD model selection click on .
-> The information dialog Generating CAD models opens.
As soon as the generation has completed, you will get informed by the note Check your emails that the component was sent by e-mail.
If you close this window, further CAD models can be selected.
Furthermore all generated CAD models are listed under Download CAD models.
After clicking on the link Info specific part information is displayed:
In order to import models into the CAD system, do the following: