Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Proceed as follows, in order to download a CAD model:
Make sure that the desired part is specified in the table view (and in the variable view in addition - if there are value range fields).
If not yet done - determine the desired CAD formats and the transfer mode to CAD in the Download area of CAD models under Edit CAD formats -> Add CAD formats. Details on this can be found under Section 4.8.2.1, “How can I select a CAD format? | How can I define the transfer mode into the CAD system? (Supplier portals)”.
Now in the dialog area CAD model selection, click on .
-> The information dialog Generating CAD models opens.
As soon as the generation has completed you can download the CAD models in this window, or directly transfer to the CAD system or you will get informed by a note that the component was sent by e-mail.
You can close the window during the generation and select further CAD models because all generated CAD models are also available in the Download area of CAD models.
In the Download area of CAD models the following links and symbols are displayed:
In addition the following is shown:
Via checkbox on the left you can select single parts or all parts (checkbox at the top) and then apply the command on these.
Detailed information about the individual modes you can find in the following subchapters.
Download: See Section 4.8.2.2, “How can I download the chosen CAD model and import it into the CAD system? (Supplier portals)”.
Direct integration: See Section 4.8.2.3, “How can I directly integrate the chosen CAD model into the CAD system (PART2cad)? (Supplier portals) ”.
E-mail delivery: See Section 4.8.2.4, “How can I send the chosen CAD model to my e-mail address and import it into the CAD system? (Supplier portals)”.