powered by CADENAS

Manual

Manual

2.3.5.1.4.  Key "CreateIMates"

You have the opportunity to configure the behavior of the interface for the creation of iMates in the document.

Enabled function allows a simplified placement at bolts, nuts, rings, washers, bearings and lock rings.

Value range: 0,1,2,3

  • 0: No iMates are created.

  • 1 [Default]: Only placement information is used in order to create iMates.

  • 2: iMates are created for all existing insertion points (behavior like in V8).

  • 3: First use placement information to create IMates (option 1), then - if not successful - create IMates for all insertion points (option 2)

Further exemplary figures:

[Note] Note

iMates are retained when using Replace parts function!