![]() |
After clicking
on the button the Edit/delete dataset
window shows up.
The button is only available with ERP functionality.
See Section 4.21.1, “ Load additional scripts - erpcustom.cfg -> Block [LOAD]”.
The data view is divided into Link-data and ERP data.
Click on the value needing to be changed, change it accordingly and click on Update dataset.
Deletes the data of the LINKTABLE.
Afterward follows an inquiry whether or nor the data of the ERPTABLE should be kept. Confirm/deny the inquiry accordingly.
Opens the window of the same name.
In the SQL command entry field you can enter any command.
Define the maximum number of lines in the result.