![]() |
In the block AttributMapping(is3d) you determine whether the PARTsolutions standard attributes (geometrical, NT, NN, LINA, etc.) and all fields of the link database (if an ERP integration exists) are to be exported to the CAD system, and if so, in which language(s).
In the following you can find the most important information for your CAD system. Basic information on attribute mapping is found under Section 2.2.4, “Attribute mapping ”.
In Inventor, these are then available under iProperties and in the BOM list.
Attribute mapping is controlled via the following blocks:
In the following the single blocks are explained: