![]() |
2.3.7.5.
Attribute mapping in Solid
Edge
2.3.7.5.3. Block
[CadDocumentAttributes] - Transfer further extra attributes
|
|
---|---|
Prev | Next |
In order to transfer further extra attributes, add the respective keys. These are displayed in Solid Edge, in the file properties on the "Custom" tabbed page.
In the block [CadDocumentAttributes], add as many further keys as you like.[62]
#:VISFGUI;1 [Custom] SpecialAttribute=?GetObject("iface.calcnameservice").start(0).Format("<ATTR(LINA)>").value()
In this example the key "SpecialAttribute" has been applied and will be transferred to the attribute "LINA" (Bom-list).
Optionally you may also define the language of the attribute.
#:VISFGUI;1 [Custom] SpecialAttribute=?GetObject("iface.calcnameservice").start(0).Format("<ATTR(english,LINA)>").value()
In order for the attributes to receive a prefix enter the following red marked row in the block [AttributeMapping(is3d)]:
[AttributeMapping(is3d)]
Attr_Section_01=Custom
Attr_CopyFrom_01=default
Attr_Prefix_01=CNS_
Attr_Content_03=ProjectInformation
...
...
Attr_Content_07=Custom
Attr_Section_07=Custom
Attr_Prefix_07=CNS_
Results in Solid Edge in the file properties on the tabbed page "Custom" .