![]() |
4.13.1.1.1. Without direct linkage to
the ERP system
4.13.1.1.1.1. Manual entry of
ERP number
|
|
---|---|
Prev | Next |
Manual input of ERP number is default setting when using the PLINKDB. When using PLDBDEMO a timestamp number is automatically created by default.[82]
Select a dataset without ERP number in order to create it and to add the dataset to the link database.
Call the dialog box new ident-no. by clicking on the button
Add dataset to link database
.
(The display of the button is role-dependent. Possibly it is not available for certain roles.)
|
Enter the ERP number (if not automatically created) and select further values in the list fields and confirm by clicking on OK.
-> The link database dataset with the fields ERP number, Material, Active status and Requested status (default) is immediately shown in PARTdataManager.