Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Do not edit the following entries! The entries are in the plinkcommon.cfg file under $CADENAS_SETUP.
Join statement defines, which primary key is assigned to which foreign key in the LINKTABLE and ERPTABLE. In this case „erp_pdm_number“.
PRJTABLE is used for the function Edit project table (see Section 4.25.7.7, “ Edit project table ”).
The TREETABLE is needed in order to display the red-green status in the directory tree. As of V9 this is necessary due to the new index structure (especially because of links).