![]() |
2.3.8.3.
Attribute mapping in
SolidWorks
2.3.8.3.1. Block
[AttributeMapping(3D)] - Set attribute language
|
|
---|---|
Prev | Next |
Under Attr_CopyFrom_00 set the desired language. The keys Attr_Content_00 and Attr_Section_00 remain unchanged.
default: The attributes are exported in the $CADENAS_LANGUAGE.
Assign language (german, english, french, etc.): The standard attributes are exported in the indicated language.
![]() |
Note |
---|---|
If there is no translation for the indicated language of the attribute, no attribute is exported (not even from the $CADENAS_LANGUAGE language). |
For copying attributes the parameters var_exclude and var_visbile=1 can be used. var_visible=1: (default) - tells the interface that only visible attributes have to be processed.
With „var_exclude“ you can assign certain attributes to an "Ignore" list.
No entry: No standard attributes are exported. (In order to explicitly export specific attributes, please see the information in the following sections.)
In SolidWorks these are displayed under File information on the user-defined tabbed page as standard attributes.