Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
4.10.
Basic
design of "new ident-no." dialog box - erpcustom.cfg ->
Block [USERDIALOG]
4.10.1.
material_assign.cfg (with ERP integration)
|
|
---|---|
Prev | Next |
In the
configuration file material_assign.cfg
you can set
which materials should be displayed in PARTdataManager, in the dialog
box new ident-no..
During the export to the CAD system the PARTsolutions material is mapped onto the CAD system material so that the physical properties can be calculated in the CAD system.
Information on the transfer of the material attribute to the CAD system can be found under Section 2.2.5, “Material mapping ”.
Information on the inclusion of the material into the file name can be found under Section 2.2.2.2, “File name: set generation options ("FileName" key) ”. Default: If a material information is available, include it into the file name.