Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the DIN, EN and ISO datasheets (as well as other country standards) certain sizes are sometimes considered to be avoided. If the option is activated, lines to be avoided are marked in the PARTdataManager Part view.
In order to show/hide parts uses the button Show/hide lines to be avoided.
Settings on this are carried out in the block [EOLService]:
LinkdbVariants: Show/hide LinkDB variants in the table
true: LinkDB variants are not basically hidden and the visibility can be controlled via .[23]
ShowLines: Show/hide the "to avoid" lines in the table
true: Lines marked with "to avoid"[24] are not basically hidden and the visibility can be controlled via .
ShowButton: Activation/Deactivation of the button
|
[23] With existing ERP integration LinkDB variants can be created via . On this see Section 4.7, “ERP toolbar and menu ”.
[24] The markup happens on the side of catalog manufacturer. On this see Section 9.8.12.2, “Mark parts to be avoided ” in eCATALOGsolutions Manual.