powered by CADENAS

Manual

Manual

1.7.5.19.4.  Block PARTindex - Report sharing

Reports are saved in the shared directory which can be set under $CADENAS_SETUP/partsol.cfg -> block [PARTindex].

There are two keys:

  • SharedIndexDir for the AppServer

    Default is $CADENAS_DATA/shared

  • SharedIndexDir(AppClient)for the AppServer Clients if a remote AppServer is used, which means that the index is used via AppServer (whenever the "Catalogs" option is used [Catalog browsing, search and database with AppServer / Catalog browsing and search with AppServer]).

Otherwise:

  • Reports and Analyses are created on the AppServer, thus are accessible for all.

    [Note] Note

    Document scan and PARTconnection will access the shared directory via file system (not via AppServer), so Clients have to have the required rights to access this path.

  • It can be set whether reports should be visible only for the creator or for all.

    $CADENAS_USER/reports.cfg

    [Common]
    ReportsVisibleForAllUsers=1

    Value range:

    • 1: Visible for all (default)

    • 0: Visible only for creator

[Note] Note

If reports existing from an earlier PARTsolutions version are not found anymore, please move them into the correct directory.