Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Standard case when using an ERP integration in PARTsolutions is adding an ERP number triggered from PARTdataManager via ERP toolbar and command Add dataset to link database. At the same time there is an export restriction for parts which do not have an ERP number.
I.e. that parts without ERP number cannot be exported to the CAD directly from the Seamless environment by default.
As of V11 SP3 it's possible to call the dialog new ident-no. in Seamless when exporting in order to create an ERP number, if not yet happened.
Hereto perform the following settings:
![]() |
Note |
---|---|
These are not dedicated settings for Seamless, but are just mentioned at this place for the sake of completeness. |
Decisive
is, that under plinkcommon.cfg
-> block
[Common]
->
key APPNAMES
the
value Seamless
is
entered.
[Common] APPNAMES=PARTdataManager,PARTproject,PARTcreatorprint,Seamless
Under
erpcustom.cfg
-> block [dialogOnExport]
-> key
default
set the
value to 1.
[dialogOnExport] default=1
Also see Section 4.11.2, “ erpcustom.cfg -> Block [dialogOnExport] - Automatic generation of ERP number: Export dialog for material and other fields yes/no ”.
Under
erpcustom.cfg
-> block [LOAD] activate the key erp_export_ts
.
[LOAD] ;Generate ERP on Export erp_export_ts=$CADENAS_SETUP/scripts/erp/erp_export_ts.vbb
Also see Section 4.21.1, “ Load additional scripts - erpcustom.cfg -> Block [LOAD]”.
Under
erpcustom.cfg
-> block [ADDTODB] activate the key erp_nrgenerator
.
[ADDTODB] #:HELP;default;Activation of the ERP Number Generator. erp_nrgenerator=$CADENAS_SETUP/scripts/erp/erp_nrgenerator.vbb
Also see Section 4.11.3, “ ERP Number Generator - erpcustom.cfg -> Blocks [ERP_NRGENERATOR] und [ERP_NRGENERATOR_CONDITIONS] ”.
![]() |
Note |
---|---|
|