Software server and the V9.03 FLM server don't have to be
installed on the same computer.
...you have purchased a
node-locked version and no X-F licenses
Check the
License Manager
...directory "$CADENAS_LICENSE" ...registry or environment
on the FLM Server computer does not point to the directory in which
the current license.cfg or default.cnsldb is
located.
The service doesn't start
or licenses are not found
Note
As of PARTsolutions V9.03
during the installation of the FLM server no registry
entries are set.
Please
check, whether still some old entries of a FLM server exist in the
registry and if yes, delete them.[17]
Service is not
correctly installed
If the
service is running even though it is set to not started, please check the above
points.