powered by CADENAS

Manual

Manual

11.5.2.2.4. Buttons
  • New

    OK In order to generate a new variable, click on the New button. --> The Generate new variable window is displayed. Enter the required name. Then complete the remaining fields and confirm with OK.

  • Rename

    OK If you wish to change the name of an existing variable, first click on the name itself and then on the Rename button. --> The Rename variablewindow is displayed. Enter the new name and confirm with OK.

  • Delete

    If you wish to delete variables, first click on the name itself and then on the button Delete .

    [Note] Note

    If you rename/delete variables, it may be necessary to rename/delete the entries of the variables in the identification or Description of geometry.

  • Standard variables

    On this see Section 11.5.2.2.4.1, “ Standard variables ”.