Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Standard variables are used for various purposes and can simply be added to the table.
Standard variables with identification type Geometry attribute are for example:
Standard variable with identification type Object attribute is for example:
Transfer order number to CAD system via standard variable.
On this see Section 11.5.2.2.4.1.1, “Transfer order number to the CAD ”.
Standard variable to mark parts to avoid:
In the DIN, EN and ISO datasheets (as well as other country standards) certain sizes (characteristics) are sometimes considered to be avoided.
On this see under Section 11.5.2.2.4.1.2, “Mark parts to be avoided ”.
Apply the order number as Standard variable in the part.
Note | |
---|---|
When exporting the part into the CAD system later, the respective Standard variables are found in the CAD system, in the file properties. |
Note | |
---|---|
You can also transfer the Standard variable CNSORDERNO via CNS classification into the CAD system. On this see Section 7.8.2.4, “ Variables ” (Variable with order number). |
In order to insert the Standard variable CNSORDERNO into the table proceed as follows:
Instead of applying Standard variables in the table, you can apply the same variables as Class variables.
On this see Section 7.8.2.5.1, “CNS classification and attributes ”.
Marked lines are displayed with the respective icon in PARTdataManager, in the characteristic attribute table. You can enable or disable the function via toolbar icon .
Default is enabled so that all project lines are displayed.
If you disable the function, lines with icon are hidden.
Tip | |
---|---|
The following markup of parts complement each other:
|