powered by CADENAS

Manual

Manual

10.5.1.  History

10.5.1.1. What are Features?
10.5.1.2. Part (name) context menu
10.5.1.2.1. Part information... (part)
10.5.1.2.2. Insert Fixed plane...
10.5.1.2.3. Exchange base planes (part)
10.5.1.2.4. Import foreign geometries
10.5.1.2.5. Dependencies... (part)
10.5.1.2.6. Search
10.5.1.2.7. Rotate (assembly)
10.5.1.2.8. Pan (assembly)
10.5.1.2.9. Mirror
10.5.1.2.10. Level of Detail
10.5.1.2.10.1. Configuration
10.5.1.2.10.1.1. Context menu commands
10.5.1.2.10.1.2. General adjustments
10.5.1.2.10.1.3. Special adjustments
10.5.1.2.10.2. Workflows
10.5.1.2.10.3. pdetailopt.cfg - Settings
10.5.1.2.10.3.1. Block MAIN
10.5.1.2.10.3.2. Block CONFIGNAMES
10.5.1.2.10.3.3. CATALOGS, DIRECTORIES, PROJECTS Blocks
10.5.1.2.10.3.4. Tabulation
10.5.1.2.10.3.5. Export of neutral formats and 2D derivation
10.5.1.3. Context menu base plane
10.5.1.3.1. Settings... (base plane)
10.5.1.3.2. New sketch... (base plane)
10.5.1.3.3. New 2-D sketch... (base plane)
10.5.1.3.3.1. Buttons in connection with New 2D drawing
10.5.1.3.3.1.1. Text
10.5.1.3.3.1.2. Polyline
10.5.1.3.3.1.3. ellipses
10.5.1.3.3.1.4. Insert hatch
10.5.1.3.3.1.5. Dimensioning mode
10.5.1.3.4. Dependencies... (Plane Feature)
10.5.1.3.5. Insert new plane... (Plane Feature)
10.5.1.3.6. Delete plane (Plane Feature)
10.5.1.3.7. Visible (Plane Feature)
10.5.1.3.8. Paste sketch
10.5.1.4. Sketch context menu
10.5.1.4.1. Edit...
10.5.1.4.2. Duplicate sketch
10.5.1.4.3. Construction sketch
10.5.1.4.4. Base
10.5.1.4.4.1. Extrude...
10.5.1.4.4.2. Rotate...
10.5.1.4.5. Cut
10.5.1.4.5.1. Extrude...
10.5.1.4.5.2. Rotate...
10.5.1.4.6. Copy (only sketch)
10.5.1.4.7. Cut (including dependencies) - Move complete history tree
10.5.1.4.8. Rename
10.5.1.4.9. Delete...
10.5.1.4.10. Show error...
10.5.1.4.11. Dependencies...
10.5.1.4.12. Visible in this configuration
10.5.1.4.13. Set mark
10.5.1.5. Extrusion and/or rotation feature context menu
10.5.1.5.1. Edit... (Base extrusion / Cut extrusion)
10.5.1.5.2. Show error... (Base extrusion / Cut extrusion)
10.5.1.5.3. Rename... (Base extrusion / Cut extrusion)
10.5.1.5.4. Delete... (Base extrusion / Cut extrusion)
10.5.1.5.5. Dependencies... (Extrusion feature)
10.5.1.5.6. Convert to cut / Convert to base
10.5.1.5.7. Set mark

Aside from the 2-D Sketcher, the History menu area is the central “scene of events” in PARTdesigner. Its context menus are used to open 2-D Sketcher and to create the components. In addition, the History documents all design steps, so that the relevant component structure can also be reconstructed and possibly modified at a later point.

Example

Open the Sketcher via the history

Open the Sketcher via the history