Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
In the dialog Rule properties, you can adjust the orientation of the pipe clip.
Again open the dialog Rule properties of the connection point "Rohrschelle".
For this, in the docking window Configurator, in the context menu of the rule "t_beam_pipe_clip", click on the command Properties.
Following operations have to be performed:
Translation: "IF PC@S2 = 78 THEN PC@S2+PC@H1/2-75 ELSE PC@S2+PC@H1/2 ENDIF"
In order for the pipe clip to be correctly positioned - meaning with the base plate on the T-beam, it still has to be shifted by the thickness of the base plate "S2" and half a clip part "H1/2". (Beforehand for "S2" and "H1" shares had been set.)
-> Now the pipe clip is properly positioned on the T-beam.