![]() |
5.11.3.
2D derivation: Create your own Combination views (*.dw)
5.11.3.10. [ELEMENT_frame] Combine more elements in
frame
|
|
---|---|
Prev | Next |
Should more than one single element be combined, the element frame is needed. This is then the parent element for all elements placed on it.
The "Frame" element is declared with "ELEMENT_" followed by a unique identification for the element.
[ELEMENT_frame]
The following attributes are available:
Provides a DXF frame for the sketch, in other words the elements are projected onto a DXF sketch.
You must indicate width and height via the DXF sketch. In this case "width" and "height" (see below) must not be explicitly entered. Quite the contrary: If "width" and "height" are indicate, the "dxf" entries are undone.
![]() |
Note |
---|---|
The corresponding *.dxf file is located in the same directory as the same-named *.dw template file. If more than one paper format is made available, several dxf files will be located in the directory and their respective *.cfg configuration files. Compare to Section 5.11.3.11, “[Formats] Different paper formats ”. |
Indicates def file in which the translations for the text elements are located. Compare to Section 5.11.3.12, “ Translations ”.
[ELEMENT_frame] type=frame dxf=default.dxf translation=default.def unit=mm