![]() |
Now create the Assembly Table Project.
Under Project selection -> context menu of hinge_asmtpl.prj, click on the command Create assembly table project.
In the list field, select that project which contains the table by which you want to control the assembly . In this example here this is "HINGEDUMMY".
So far you already adjusted the table of "hinge_dummy.tab/tac" the Standard name is correct.
In order for only the Assembly Table Project to be visible in the PARTdataManager, and not the "intermediary steps" assembly template and assembly configuration, hide these with Hide project in the context menu of the directory tree. And also hide the dummy project in this way.
-> Now you can select the single parts "Wing" and "Bolt" and the Assembly Table Project "Hinge" in PARTdataManager.
Transfer the assembly to a CAD system (as in the example below with two different angularities).