Basically you can activate this function.
However the following warning notice always shows up:
If there are problems with the building of an assembly, check if it is possible to avoid the error by deactivating the check box.
Append free connection points automatically
This feature does not concern the Assembly Table Project since clarity is warranted in the steering table anyway. However the template, which is the basis for the Assembly Table Project, should have been created in the below mentioned way.
Assembly Configuration and Template
Prerequisite for the use of the option: Conditions ensure that there is only 1 row available per connection part.
There is no damage, if the option is activated, even though the terms are not met; but an automatic buildup is then impossible!
If there is no pattern, this option is irrelevant.
If there are patterns and the option is not activated, then at patterns no further assembling will take place.
Concerns assembly configuration and templates. With the Assembly Table Project there is no access to the single parts, since these are controlled by the table.
After activation, the corresponding context menu item is grayed out.
Currently only supported by Inventor. The interpretation can be found in CAD.
extended attributes -> PSOL_MULTISOLIDPART 0: Zu einem Teil verschmelzen 1: Als Baugruppe exportieren z.B. EXTATTRVAL{ NAME{ "PSOL_MULTISOLIDPART" } VALUE{ 0 } }
Invalidate changed tables even if the chosen line is still available.
Export single part assemblies as single parts
In case the assembly is comprised solely of one part, it will be exported as a single part.