![]() |
3.4.2.
Check ERP-Mapping (Add ERP-Mapping... and Edit ERP-Mapping...)
3.4.2.1.
Change of folder
structure, project names and paths
|
|
---|---|
Prev | Next |
The folder structure of a catalog should not be fundamentally changed after the first publication. Especially a change of the structure and a change of the projects at the same time is very critical, because many end-media and interfaces base on the originally created structure. The “regular” add of new folders / projects is no problem. The same rule is also valid for the naming of the projects (NN/NB) – if they are changed the reference in the ERP system could get lost.
A detailed description which changes need a verification, can be found under Section 6.10.4, “The most important use cases ”.