powered by CADENAS

Manual

Manual

5.13.10.15.10. Associated Part [CNSELEK|5|4]

Accessory parts are defined in two sections. On the one hand there is the usual PSOL accessory solution (PARTproject -> tabbed page Links -> Links to parts) and on the other a mechanism that links accessory data with the electrical classification.

Example: Phoenix Connector with 4 Crimp Connections. In each Crimp connection, principally a whole string of different pins with specific article number can be plugged. These are not necessarily identical for each connection.

Approach:

  1. At the Base part, set all Mounting Points needed for the accessory parts.

  2. On each connection point, set the class Mounting Point (CNS_CP|4|6).

  3. Assign the feature Accessory ID with a unique value using following syntax:

    CNS_CP|4|6||<Instanz>

    Dialog "Class variables" -> Class "Mounting Point" (CNS_CP|4|6) -> Feature "CNS_ACCESSORYID" here with exemplary value "CNS_CP|4|6||34"

    Dialog "Class variables" -> Class "Mounting Point" (CNS_CP|4|6) -> Feature "CNS_ACCESSORYID" here with exemplary value "CNS_CP|4|6||34"

    Dialog "Published Elements" -> Class "Mounting Point" -> Feature "Accessory ID" here with exemplary value "CNS_CP|4|6||34"

    Dialog "Published Elements" -> Class "Mounting Point" -> Feature "Accessory ID" here with exemplary value "CNS_CP|4|6||34"

  4. In PARTproject, on the tabbed page Links, under Links to parts, set an entry with Path to accessory part and Id, showing exactly the same value as feature CNS_ACCESSORYID under class Mounting Point (CNS_CP|4|6).

  5. At accessory part, fill out the essential information in CNSELEK|5|4.

    Classification of accessory part

    Classification of accessory part

    • Feature Parent classType gets the name of respective classification.

    • Feature Parent class instance gets the instance of respective classification.

    • Feature CNS_ACCESSORYID gets again the same unique identifier string as at base part and in this way is linked with the PSOL accessory path.

      CNS_CP|4|6||<Instanz>

      One possible form of CNS_ACCESSORYID is the concatenated string of Parent class Type and Parent class Instance.

    • [Note] Note

      The manufacturer name will be automatically entered later via PSOL-Framework.

Details on this can be found under Section 5.13.10.8, “Accessory parts (Associated Part [CNSELEK|5|4])”.