![]() |
Now the T-beam shall be taken into the Assembly.
Define a rule for the connection between "dummy starter part" and "double T-beam".
At the connection point of the dummy starter part (cp_dummy_tbeam), call the context menu command New rule.
As
connection part, select the T-beam (din_1025_s
) and as
connection point IP1
.
Activate Reverse direction and Exclusive, in the list field, select Permit automatic build.
In the docking window Assembly, insert the T-beam.
Currently an error message will still appear, because a definition is missing which characteristic of the T-beam has to be chosen for which table row in the dummy starter part. An assignment between the two tables is missing.
The problem can be solved by adding a respective rule. See next section.