![]() |
Use feature based Sketcher for new sketches: Setting not relevant anymore.
Start only one instance of PARTdesigner: If this option is enabled then it is not possible to start several PARTdesigner sessions at the same time.
Put decimal place on number block: This option shifts the comma key of your keyboard to dot. That means, when using the comma key you will write a dot. This is advantageously, because writing decimal numbers in PARTdesigner requires dots (3.5 mm) instead of commas (3,5 mm) basically.
Once the option Activate is enabled, the geometry is automatically saved in adjustable time frames. Specify the desired interval-Timeframe in minutes.
The colors defined here are displayed in the Variable Manager under Save location (compare).