Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Up to now a customer administrator had to perform a mapping for LinkDB datasets at each catalog update, if projects or variables had been changed, which led to lots of effort on the customer side and less upgrades to latest catalogs.[34]
In order to relieve the customer side, as of V10, mapping information is created in the SVN catalog status and during publishing integrated in the CIP file so that it can be processed during the installation. That means, mapping tasks are now done by the catalog modeller and don't have to be conducted on the customer side at each update.
Note | |
---|---|
For each new catalog release ERP mappings have to be created by the modeling in PARTproject. Publishing without this mapping information is not possible. |
On the customer side, a version has to be installed for which mappings have been created.
Now the new method takes effect and manual editing is only necessary in exceptional cases, if an adjustment cannot be processed automatically.
At catalog xy the latest status is from 01/01/2015 and still without mappings. A customer with V10 has exactly this catalog status.
Now a new version is released on 06/01/2015. In this, the modeling has already added the mapping information, namely at the last released status from 01/01/2015.
When the customer installs the latest status now, these mappings are automatically processed.
However, if the customer has an installed status from 10/01/2014 then therefor no mappings exist and if he installs the status from 06/01/2015 then he has to do the mapping himself (for this last time). However, parts which have not been changed between 10/01/2014 and 01/01/2015 can automatically be mapped.
[34] Hereto the Update manager is used. Call up via PARTlinkManager -> Extras menu -> Update manager. Details on this can be found under Section 5.15.2, “ Catalog update with ERP integration - Update manager ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.