Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the following the procedure of an offline catalog update is explained.
If under Catalog update -> Online, you deactivated the option Install after download, then the downloaded catalog cip files can now be found in the temporary Download directory, which you determined in the settings dialog.
Open the CIP file by clicking on (selection in an Explorer window).
-> The dialog box CIP Installation with the options and opens:
It is checked whether there are datasets with status to check and/or not mapped.
If datasets with status to check or not mapped are found during a test run, in the dialog box CIP Installation the tabs Protocol, ERP Status and PLM Status are displayed, otherwise the installation is immediately performed.
On the tabbed page Protocol the number of datasets per Status is listed.
For all affected ERP numbers the status (successful, expired, to check and not mapped) is displayed, furthermore old path, new path, old NB and new NB.
Dialog box "CIP Installation" -> tabbed page "ERP Status" / Example with status"to check", "successful" and "not mapped"
If, in the dialog box CIP Installation the tabs Protocol, ERP Status and PLM Status are displayed, then there are datasets with status to check and/or not mapped.
That means editing with the help of Update manager [37] is necessary. This status can only occur if no ERP-Mapping on the side of catalog modeling had happened.
If the installation shall be performed now after the test run, check the desired catalogs and click on , otherwise on .
If there are no datasets with the note to check or not mapped the installations runs through without further note. Then, at the end of installation the tabs Protocol, Status and ERP Status are displayed again - this time in the standard dialog area under Catalog update -> Offline.
The installation is immediately started. At the end of the installation the tabs Protocol, Status and ERP Status are displayed - this time in the standard dialog area under Catalog update -> Offline.
Result after processed installation:
At the end of the installation the tabs Protocol, Status and ERP Status are displayed - this time in the standard dialog area under Catalog update -> Offline.
The tabbed page Protocol is opened by default.
By default, on the tabbed page Protocol, the note There were mapping problems in the LinkDB. Please correct these in the UpdateManager. is displayed. At the first catalog update with V10 or V11 the mappings still have to be manually created for a last time (with the Update manager), but after this the new method is effective and manual editing is only needed in seldom exceptional cases if an automatic update is not possible.
On the tabbed page Status, you can find a detailed listing of the individual projects.
On the tabbed page ERP Status you can find a listing of all ERP numbers with its update status (successful, expired, to check and not mapped), furthermore old path, new path, old NB and new NB.
By default, on the tabbed page Protocol, the note There were mapping problems in the LinkDB. Please correct these in the UpdateManager. is displayed. When clicking on the link "Update manager" it is opened.
You can simply check whether there is something to edit: In the Update manager deactivate the button Show mapped lines.
If everything could automatically be assigned, then nothing is selectable anymore. Otherwise perform the mappings with the help of the Update manager.
REQUESTED_STATE is set on Expired at the old version and on Updated at the new version.
ACTIVE_STATE is on Locked after the update both at the old version and at the new version.
If in the ERP set of rules the variable ACTIVE_STATE is used, then administratively set the new version's status on Released.
Further you have the possibility to fetch information on changes before the catalog update (even if only the status successful and/or expired occurred, meaning no editing in the Update manager is necessary.
Again, in the dialog box the tabs Protocol, Status and ERP Status are displayed.
On the tabbed page Protocol an overview is shown, subdivided by the following categories:
On the tabbed page Status you can find a detailed listing of the individual project's status.
On the tabbed page ERP Status you can find a listing of all ERP numbers with its update status (successful, expired, to check and not mapped), furthermore old path, new path, old NB and new NB.
[37] Detailed information on Update manager can be found under Section 5.15.2, “ Catalog update with ERP integration - Update manager ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.