powered by CADENAS

Manual

Manual

6.9.3.11. Resolved value range

Value ranges are automatically resolved. In many cases the resolving is correct, in very complex cases possibly a manual editing is required to receive a correct mapping.

The following example shows a standard case with correct resolving of the value range.

The right table shows all single lines of the resolved value ranges.

The right table shows all single lines of the resolved value ranges.

To be sure that correct mappings are available, perform the function Map resolved value ranges .

  1. Above the table, click on the button Map resolved value ranges (for all table lines).

    or on the context menu command Map resolved value ranges of this line of a single line.

    Context menu command "Map resolved value ranges of this line"

    Context menu command "Map resolved value ranges of this line"

    -> The dialog box Select value range variables opens.

    There are checkboxes for all value range variables.

  2. Activate those checkboxes where the value range has been resolved and confirm by clicking on OK.

  3. Now, in a line, click on the icon Map resolved value ranges .

    -> The dialog box Edit value range mappings opens showing a listing of all value combinations (single values separated by semicolon). At the end of each line you can find the LINE_ID separated by a colon.

    The LINE_ID can also be found in the right table as last column.

  4. Confirm with OK.

    Now, when changing values of value range variables in the left table, in the right table, the correct line is automatically selected.

  5. If all mappings are correct, click on Verify all mappings .

[Note] Note

If certain value combinations should not be correct, you can simply perform changes with the help of the LINE_ID (last parameter behind the colon).

[Note] Note

If certain value combinations are not existing anymore in the new catalog version, set the respective LINE_ID on the value '-1'.

Dialog box "Edit value range mappings"

Dialog box "Edit value range mappings"

Check: When selecting not existing value combinations in the left table, there is no display of the right table.