powered by CADENAS

FAQ Options

FAQ Information

FAQ Categories

Categories:

FAQ Description

How can I use the PARTsolutions license on a new computer?

1. Please use the form which can download with the following link:

    Hardware exchange 

2. For licensing the Host-ID (MAC address) of the old and the new computer is required. 

    ->  The Host-ID can be selected in the license manager PARTadmin.


 

3. Get further help regarding licensing by clicking F1 within PARTsolutions

 

 

 

 

 

 

 

 

 

100% users marked this FAQ as helpful.
|
Was this answer helpful?
2 votes