Pipe Fittings | Western Steel Agency
A Pipe Fitting is intended to be welded on the spot at its ends to attach it to the pipe along and permit an amendment in direction or pipe diameter also branching and ending. This fitting becomes a part of a system for transporting fluids in a very safe and economical manner, over short or long distances.
Western Steel Agency is one of the most leading Pipe Fitting Manufacturers in India. One of our popular products in the Metal Market is Pipe Fitting End Caps. We are an ISO 9001:2008 certified company with existence in the Metal Market since 2007. Western Steel Agency is one of the leading Pipe Fittings Suppliers in PUNE and Pipe Fittings Suppliers in Mumbai.