powered by CADENAS

Array

Pin Source

Also from manansteel.com

Social Share

Pin Details

Pinned January 8, 2022 via web
EN24 Round Bar Manufacturer in India - Manan Steels & Metals - ISO 9001:2015 Certified Company
Manan Steels & Metals is one of leading EN24 Round Bar Manufacturers, Exporter and Suppliers in India. EN24 Round Bar is made of pure medium carbon steel and has a ductile strength that is comparable to mild steel. EN24 Carbon Steel Bar is suitable for a wide range of manufacturing applications requiring high strength, such as the production of tubes, studs, bolts, connecting rods, screws, and rollers.
  • 428 views
  • 0 likes
  • 0 comments
  • 0 repins