Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
For the automatic assignment a process has to be created.
In the context menu of Workspace -> Processes -> Article Assignment, click on the command Add new process.
Click on the
button Load predefined template
and then on the template Dimension search.
Select the single nodes one by one. Thereby the respective setting options are displayed. The respective selection is marked in yellow. In red nodes you have to perform settings mandatorily. In green nodes further settings can be made optionally. A complete green pipeline may be executed.
Fields from catalog containing the standard number (e.g. ISO 1234):
Select the attribute (or several), which contains the Standard number and move it to the right via arrow key. Confirm with .
-> Selected attributes are displayed in the input field now.
PARTsolutions catalog: In the same way as above, determine the desired catalog via search button .
Select the node Line Finder NENN and determine the attribute (field) for Dimension and Material with a click on the search button .
Click on the Start button to execute the pipeline.
-> In the docking window Performance a respective message is displayed.
Optionally,
save the process. In this way you can call it anytime and use it again
(possibly modified). Click on the respective icon .