![]() |
A small
example for setting the import path of an item (using pdmProxyPdmDocumentI
).
Create a
VBS filter node
directly after the Conversion service (meaning before the converter has been processed). Set
VBS file
(plugin_template.vbs
) and
VB Class
(_AfterConversion
).
Go to the function „AfterConversion“
Add the following lines of code:
dim docProp = item.GetPropertiesObject() dim pathProp = Application.GetObject("pdmProxies.ObjectFactory").createPdmProxiesObject("pdmProxyPropertyObjectC", "Testpath/test") pathProp.setType("STRING") docProp.setProperty("path",pathProp)
Get the root properties object (Return value pdmProxyAttributeContainerC)
dim docProp = item.GetPropertiesObject()
Create new pdmProxyPropertyObjectC & setValue and Type
dim pathProp = Application.GetObject("pdmProxies.ObjectFactory").createPdmProxiesObject("pdmProxyPropertyObjectC", "Testpath/test")
pathProp.setType("STRING")
Add pdmProxyPropertyObjectC to pdmProxyAttributeContainerC
docProp.setProperty("path",pathProp)
The
converter.vbs
(processed
during AttributeMapper) converts this attribute „path“ to
a classification of the product.
In classification: |
"Name": "path", "Group": "document", "Value": { "Text": "Testpath/test" }, "Id": "path" }, |
Edit Structure Node in PARTdataCenter
Document Path: $document::path.
(Group: document; Name: path --> see Classification PARTdataCenter)
Depending on which function is used in the code, the proper group has to be chosen in the Structure Node:
dim docProp =
item.GetPropertiesObject() -->
Mapping of functions to groups:
GetPropertiesObject() | --> document |
GetFileProperties() | --> file |
GetCadAttributes() | --> cad |
GetCadDimensions() | --> dimension |
GetPdmAttributes() | --> pdm |
GetCustomAttributes() | --> custom |