![]() |
The following two examples will show the use of the two mentioned templates.
The goal of the two examples is always the same: Building catalog structure = Setting import path for the item.
You will see that the approach is different in the two examples but the result is the same.
If there’s a
choice always work with pdmProxyPdmDocumentI
(example 1),
because the values in there can be stored in a XML file. This XML file can
be taken as input for a new pipeline. The other approach is not
persistent. It can not be saved in any file. If an error occurs in the
pipeline / program, the data is lost.
The explanation of both options is given just for the sake of completeness.