Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
1.4.3.
PARTapplicationServer Dashboard - Tasks
1.4.3.1. Dashboard
display: Preconditions and call
|
|
---|---|
Prev | Next |
In PARTadmin -> AppServer client -> tabbed page Settings, under AppServer connection, one of the following options has to be selected:
Server address: Enter name or IP address of Server (which is running as Service).
(For
testing purposes "localhost" can also be used. For this, start the
locale pappserver.exe
via
command line with parameter "-e".)
Click on the button Show server state.
-> The tab <"Address of Server"> (in above example "localhost") shows up beside the Settings tab.
Optionally you have the opportunity to activate the option Use external browser.
Log in under User, if not automatically done. The most easiest is to use the option User System Credentials.
Select the tabbed page Tasks and click on New task.