![]() |
For older versions, may be use at a single workstation is not provided for Article assignment. If this is the case the following preconditions have to be fulfilled.
Installation of PARTsolutions and the respective catalog (e.g. Standard catalog)
On the
installation medium, under tools\databases\Partwarehouse
you can find the file create_tables.sql
.
Under
$CADENAS_SETUP\partwarehouse
,
in the configuration file pwserver.cfg
, enter the
connection string.
ConnectionString=DRIVER={SQL Server Native Client 11.0};UID=pwserver;LANGUAGE=us_english;DATABASE=PWServer;WSID=PROG-DEV091;APP={Microsoft® Windows® Operating System};
SERVER=TINPWTEST02;Uid=pwserver;Pwd=start1234;
Under
%cadenas_setup%
-> “pappserver.cfg
” make the
following adjustments:
Search for the key “Services” and add the value “PartWareHouseService” as last value separated by comma.
Services=all,AnalysisService,PartWareHouseService
Under
%appdata%\cadenas\partsolutions
edit the configuration file partdatacenter.cfg
:
When working at a local workstation, in PARTadmin -> category AppServer client, select the option Use local AppServer.
Under Workspace, click on the context menu command Set remote connection. (If the command is not displayed, possibly restart the computer.)
-> The dialog box PARTdatacenter Classify server is opened.