Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Value range fields can also be show in PARTdataManager.
Value range fields can be defined as:
In order for the value range field to be shown in color and work according to plan in the PARTdataManager, you must set the following:
In the columns ATWITHLIST (value list) and ATWITHRANGE (value range) set an 'x' for the desired class name (CLASSNAME) and attribute name (ATTNAME), if you wish to have this function.
If a list of values is desired then apply the corresponding row several times.
In the following figure matnr6 is applied three time with the attribute 'L' (under ATTRIBUTE_NAME). The displayed value is located under ATTRIBUTE_FL_VALUE, since we are talking about a floating number value; with a text the entry must occur under ATTRIBUTE_VALUE.
If a value range is desired, the enter the maximum value in the ATTRIBUTE_FL_MAX_VALUE column.