Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
At Full-text search projects and link database are always searched together. Even if several search terms are entered it doesn't matter whether hits result from the project file (geometry data) or from a link database column.
The table shows hits both in the project file and in the link database.
In this example search terms are used, which are linked with the boolean operator OR [102].
The characteristic again is, that the one terms will achieve hits in project files, the other in the link database.
gasket OR o-ring
With OR it is sufficient, if one of the terms scores a hit.[103]
That means: Projects are found, which either have the term "head cap bolt" OR the term "awesome", regardless of whether the term is in the project file or in a LinkDB column.
The hit list contains head cap bolts, of course, but also a hit "hexagon bolt".
The reason is, that the project with hexagon bolts has an entry "awesome" in the link database.
Note | |
---|---|
Please keep in mind - especially when manually adding a term into the link database, that the ERP index has to be created again.[104] The respective command is found in PARTadmin -> Index administration -> context menu command Create link database search index. The blue database icon signalizes, that the ERP index is available, otherwise the icon is grayed out.
|