Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Have a look on the catalog and project data directly in the project selection downright.[53]
Do you want to display all available part information?
-> To expand the section single-click on the icon in the top right corner.
Then more information like company address for example is displayed.
On project level catalog and project information is displayed.
On all levels the TagCloud is displayed.
The TagCloud contains the most frequent catalog terms. When you click on a term a keyword search is performed. If an ERP integration is available, then optionally also ERP full text search .
By default the first 20 terms of the TagCloud with at least 3 characters are displayed.[54]
This section can be customized and contain still more information.
In the following you can see a few exemplary figures:
The project information also shows the classification. Scroll down in order to see all information.
Further additional information on project level
The AFAG catalog for example shows the addresses of subsidiaries together with a map.
If available you can switch to Google StreetView.
The views are HTML pages which are created with a template. The templates can be customized.
[53] Under PARTdataManager -> Preferences... menu -> Part selection -> Show details window you can control the visibility of this dialog section.
[54] Adjustable via configuration file. See Abschnitt 1.1.6.5.6.6, „Block [InfoPane] - TagCloud“.