Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following 2D CAD formats and 2D system neutral formats are available:
At each format the existing tabbed pages are listed. With click on the link you can reach the respective section.
See tabbed page Views, tabbed page Filter, tabbed page Layers, tabbed page Export options
See tabbed page Views, tabbed page Filter, tabbed page Layers, tabbed page Export options
See Views tabbed page, Filter tabbed page, EPS Drawing Options tabbed page
See tabbed page Views, tabbed page Filter, tabbed page Export options
See tabbed page Views, tabbed page Filter, tabbed page Layers, tabbed page Export options
See tabbed page Views, tabbed page Filter, tabbed page Layers, tabbed page Export options
For each format the available tabbed pages are listed. With click on the link you can reach the respective section with further information.
See tabbed page Views, tabbed page Filter, tabbed page Layers, tabbed page Export options (insertion position, line attributes)
See tabbed page Views, tabbed page Filter, tabbed page Layers, tabbed page Export options (insertion position, line attributes)
After the export, the file can only be opened from your CAD system and is available for further editing.
Detailed information on the Shortened view option is found under Section 3.1.1.11.3.1.4, “ Alternative 2D size Optimize drawing view on paper size / ”.
You can export all listed views or only the selected ones. Choose a mode:
If under Source the option Selected views has been selected, you can activate the desired views via checkbox under Views.
You can find detailed information on the individual Views under Section 3.1.1.11.3.1, “ "2D view" dialog box ”.
The following two figures show the default case: No unit conversion is processed during the export. The dimensioning values are identic in the 2D derivation of PARTdataManager and 2D CAD system.
On the tabbed page Filter you have the following options available in the list field:
Insertion position: The insertion position in the CAD system can already be set in PARTsolutions - assuming your CAD system supports this function. Enter the X and Y coordinates.
No Attributes : ...prevents certain attributes (for example texts from PARTproject) from being transferred to the CAD system during export
Per default, the settings are set to by layer. Color and line settings depend a) on the layer settings in the CAD system or b) on the settings on the tabbed page Layers. In the list fields, you can explicitly select other settings for lines and colors, which then override the layer settings.
Insertion position: The insertion position in the CAD system can already be set in PARTsolutions - assuming your CAD system supports this function. Enter the X and Y coordinates.
No Attributes : ...prevents certain attributes (for example texts from PARTproject) from being transferred to the CAD system during export
Aside from the possibility of directly assigning lines and colors, the color and line settings may also be made dependent on the layer setting in the CAD system. For this, select the option "by layer".
During export in the EPS 2D format you have the following setting options on the EPS Drawing Options tabbed page:
The page size adjusts to the bounding box of the part. Thus the input fields for Width, Height and the option Adapt to page size are inactive.
Meaning, if for a mm part the unit inch is selected, the value becomes smaller; the opposite happens, if for an inch part the unit mm is selected.
The part adjusts to the page size. (The opposite of Minimum size)
Scale: 1 = 100% | smaller or larger values than 1 are possible
No Attributes : ....prevents certain attributes (for example texts from PARTproject) from being transferred to the CAD system during export.
Aside from the possibility of directly assigning lines and colors, the color and line settings may also be made dependent on the layer setting in the CAD system. For this, select the option "by layer".
Insertion position: The insertion position in the CAD system can already be set in PARTsolutions - assuming your CAD system supports this function. Enter the X and Y coordinates..
No Attributes : ...prevents certain attributes (for example texts from PARTproject) from being transferred to the CAD system during export.
Aside from the possibility of directly assigning lines and colors, the color and line settings may also be made dependent on the layer setting in the CAD system. For this, select the option "by layer".
Insertion position: The insertion position in the CAD system can already be set in PARTsolutions - assuming your CAD system supports this function. Enter the X and Y coordinates..
No Attributes : ...prevents certain attributes (for example texts from PARTproject) from being transferred to the CAD system during export.
Aside from the possibility of directly assigning lines and colors, the color and line settings may also be made dependent on the layer setting in the CAD system. For this, select the option "by layer".