The columns themselves are ordered as
set under Bill of material menu -> Order of columns (see figure).
In this menu, you can move the relevant
marked column by
Drag & Drop
or using the arrow buttons. The topmost position in
the list corresponds to the left-hand column of the Table view.
If you want to hide a Column in the Table view, simply remove the
respective checkmarks.
Via
use as standard you can set whether the
currently set order and selection for this
form type (e.g. "Neutral") should be set as a presetting for
files applied in the future.
Note
The total price for part lists with more than
one total price row, is usually automatically calculated at the lower
end of the table. This is only possible however if the price is
entered in all total price
rows.