You can use any 3D file as search part:
In the History section, select the 3D files tab.
A number of formats can be opened: [51]
|
When selecting the STEP format the dialog box Import options for format STEP file input is opened.
If there is an ambiguity for a file extension, an additional dialog box appears.
Ambiguities
are possible for a file extension such as .prt
for example, which is
used by Creo Elements and NX as well, furthermore for several versions
of a CAD system.
In the list field select the desired system and the desired version.
Then the dialog box Selection of unit is opened.
In the list field, select the correct unit: mm, cm, dm , m, INCH, FEET, INCH/10, INCH/100
-> The file is loaded in the dialog box on the left side. On the right side the part is shown in the 3D preview.