Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
3.1.12.5.4. Examples
3.1.12.5.4.5. Example 5 -
Primary meaning of the Bolt before other components
|
|
---|---|
Prev | Next |
Project "CSN 02 1431" (Nut) is displayed in green in the connection dialog since it contains at least one row with an ERP link (see green status light in the table). It has nominal thread diameter "27" and the pitch "3" (see table).
However there is no green value in the connection dialog.
This is due to the fact that no ERP link exists for any of the Bolts for nominal diameter "27". The bolt however is the basic component of connections.
Therefore it is correct that no green value is displayed.
![]() |
Note |
---|---|
Due to the primary meaning of the bolt it is useful to first select the bolt when creating a connection. |