Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Goal: Select a bolt with "Nominal=30" and "Length=100"
Selection of the green bolt project "DIN 7968" and nominal value "30"
-> The desired length is displayed in orange.
=> Without a change to the selection made thus far, it is not yet possible to get a green length of 100.
The likewise green bolt project "GOST 7795_70" is chosen.
Test: Remove filter at "GOST 7795_70".
->The value "Nominal=30" remains orange.
Since the only set filter is at "Length=100", you recognize that for the combination "Nominal=30" AND "Length=100" there is no green path. One would have to remove at least one more filter (which is not possible) in order to get the "30" to green (according to the definition of the status color orange).
A further possibility to quickly recognize whether a green value exists, is to pin "Nominal=30" and "Length=100".
Now all bolt projects turn to orange.
The orange directories signal that although they contain an ERP connection, however not that needed with nominal "30" and length "100".
If a strict export regimentation is used, a new, fitting ERP link must be set. See Section 3.1.12.5.1.1, “Save single part ”.