Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The PARTrenderManager enables to create images on a central server, so that different workstations can access.
Server and Client application are combined in one program. The first transfer parameter ("-server" or "-client") defines the program's functionality.
For the server a directory is needed, where the temporary files are stored. This directory has to be declared by a global variable with the name "PRM_TEMP"!
The client
needs some data from the configuration file prendermanager.cfg
, which
should be inside the directory "$CADENAS_USER". If this file is not
existing at the first start there, the program will create a
configuration file with default values.
The program used for the image calculation (here the Maxwell Renderer), has to be already installed!
The user interface main component is a list, where all jobs of the currently connected server are displayed.
This list is automatically updated in a certain interval. Below the list you see some buttons to create or delete jobs for example. In addition you can call these functions via the job menu.
Furthermore beside the buttons information concerning the connected server or the file transfer are displayed.
The single orders from clients to the server are called "Jobs". These jobs contain the following data:
Already finished jobs (information on this transferred by the server) are displayed at the first positions. Then the currently processed job is displayed, and finally the waiting jobs, which not have been calculated images yet. The index numbers the complete list serially and is only important for the waiting jobs, because the sequence can be changed by it. The index number can be changed by double-click and in this way a job can be moved upwards in the list, so that the job is earlier processed by the server.
Index | Job | User |
7 | job1 | finished job of C |
8 | job2 | finished job of C |
9 | job3 | this job is currently processed by the server |
10 | job4 | A |
11 | job5 | A |
12 | job6 | B |
13 | job7 | A |
14 | job8 | A |
15 | job9 | A |
16 | job10 | B |
In this example user A can move job9 maximally to index number 13, because job6 belongs to another user. Job5 can be moved maximally to the index number 10, because otherwise it would be higher than the currently processed job.
This number serves for the job identification and is assigned by the server to each new job, which is delivered by a client. The ID has no relation to the index or the sequence and cannot be changed when a job is created.
The description helps to understand the content of jobs and to recognize jobs. Via double-click on a description it can be changed subsequently. However it is only possible as long as the job has not yet been processed and belongs to the respective user.
The sampling rate determines the number of runs the renderer can perform to calculate the images of a job. The higher the value the more exact the calculation and so the image quality. A high value results in a long calculation period for each image. After the creation of a job this value can be adjusted by a double-click. As with the description there is the restriction that it concerns the user's job itself and the job is still in the waiting line.
The status signalizes whether there is still a job in the waiting line or is currently processed by the server or is already finished. At finished jobs the number of images is displayed in addition. At the currently processed job the number of already finished images and the total number is displayed.
In the menu Server all available servers, which are loaded from the configuration file, are displayed. The server connected to the client is marked. Via click on another server it is tried to change the connection to that server. When you want to add a new server to the list, click on then menu item Add server... A dialog box opens. In this dialog the needed information (IP address, port and name) has to be entered. Thereby it is automatically checked whether the server name is unique and differs from the already existing server. A click on the button checks, whether a connection to the server is possible. This test is automatically processed before the adding of a server, if the connection has not been checked before. Only a successful test results in adding the server to the list. Furthermore you can define, whether the client shall immediately connect to the new added server. After a successful creation of the server its data is saved in the configuration file.
You can call up the PARTrenderManager in different ways:
via PARTdataManager -> menu Export -> Export in file -> Image formats -> Maxwell Render -> Maxwell Renderer tabbed page-> Render menu item -> selection Transfer to server
via PARTdataManager -> context menu of a directory/project in the index tree -> Generate image data/preview images -> Maxwell Render -> Maxwell Renderer tabbed page -> Render menu item -> selection Transfer to server
More information is found under Section 3.1.9.3.3.6.2.4.3, “Create job in PARTdataManager via Generate image data/preview images ”.
The creation of jobs in the PARTrenderManager (Client) happens in the Create a job dialog box.
Select the desired sampling rate in the list field.
Preview images showing the different qualities will help to choose an adequate sampling rate.
At this value choose an adequate compromise between quality and needed creation time.
When all settings are done, click on the button . The data is sent to the server now.
If the files are located in different folders they have to be added to the file list separately! When the finished images are resaved PARTrenderManager keeps the folder structure.
The job contains the following files:
C:/FolderA/File1.mxs C:/FolderA/FolderA1/File2.mxs C:/FolderB/File3.mxs C:/FolderB/File4.mxs
If as target directory that path which all files have common (here in the example this would only be „C:/“) is set for the resaving, then the images are saved to their respective .mxs files.
C:/FolderA/File1.mxs C:/FolderA/File1.bmp C:/FolderA/FolderA1/File2.mxs C:/FolderA/FolderA1/File2.bmp C:/FolderB/File3.mxs C:/FolderB/File3.bmp C:/FolderB/File4.mxs C:/FolderB/File4.bmp
If another target directory is set, then the folder structure is also kept (only the common path changes).
Target directory shall be: D:/Images/
C:/Images/FolderA/File1.mxs D:/Images/FolderA/File1.bmp C:/Images/FolderA/FolderA1/File2.mxs D:/Images/FolderA/FolderA1/File2.bmp C:/Images/FolderB/File3.mxs D:/Images/FolderB/File3.bmp C:/Images/FolderB/File4.mxs D:/Images/FolderB/File4.bmp
The mxs files are still under "C:/" (thus exactly in the origin paths), only the images are saved under "D:"!
Via Export in file (a single file) a job can be created directly from PARTdataManager and transferred to the server.
After a part has been loaded in the Part view, start the export via Export menu -> Export in file -> Image formats -> Maxwell Renderer.
-> The Export using Maxwell Render format dialog box opens.
Settings in the Export using Maxwell Render format dialog box:
A description on all other settings is found under Section 3.1.9.3.3, “Maxwell Render 3D ”.
-> After confirmation with the job is sent to the PARTrenderManager Client and the PARTrenderManager dialog box opens. The job appears in the dialog box. The Create a job dialog is not called. The description is automatically created. The sampling rate can optionally be changed as long as the job is in the waiting line, meaning the job status is "Waiting". The list of jobs cannot be changed anymore.
|
|
The *.mxs files are created and a job with paths to all project files is generated and sent to PARTrenderManager.
Note | |
---|---|
During the generation there are no previews available (neither the old ones, nor the new ones). [81] |
If you had selected Start renderer, then the new preview images are available as soon as the renderer has finished.
If you had selected Transfer to server, then the new preview images are available when these have been downloaded from the server and been resaved.
In the dialog box of PARTrenderManager you can see under description, for which directory the preview images have been created. Resave these in the respective directory (directories), when the job has finished.
When you want to delete one or more jobs, then select the respective jobs from the list and click on the button .
Jobs from other users, which are also selected, will not be deleted.
When deleting the current job the following has to be regarded:
The renderer can not be stopped by the server, meaning that the renderer will finish the calculation of the current image in any case. When the job is deleted during the calculation no calculation of a new image will be started by the renderer and the next job in the waiting line is processed. So it can happen, that the list of the client contains no job, which is currently processed by the server.
It is possible to request the current status of the image as preview during the calculation:
For calling the preview image there are several ways:
The preview image is displayed on the client and can be closed with a click on the image.
As soon as the renderer has calculated all images of a job, the job is marked as finished and the images can be downloaded to the client computer. Thereto you only have to select a job and click in the job menu on Save images. Alternatively you can click on the button or use the respective context menu command of the respective job line.
When the files from which the images have been calculated are from different folders, then the folder structure is regarded at saving.
Basically
each user has only the authority to change or delete jobs of his own.
When resorting his waiting jobs he cannot place them before other users
jobs. However there is the possibility to extend the user rights. In the
configuration file $CADENAS_USER/prendermanager.cfg
in
the section "global" you can find a key "role". If you set the value to
"Admin" and restart the client you can change, delete or resort all jobs
without restrictions.
[81] The reason is, that the mxs data is not saved in an own „*.mxs“ file, but in the same-named .bmp file. Preview images are stored under $CADENAS_DATA/23d-libs in the respective directory. To that place you save them after the creation.