powered by CADENAS

Manual

Manual

3.1.7.  Part view

In the Part selection, once double-clicking a project (for example part or assembly , the interface changes to Part view.

In the part view you can specify the characteristic of the part.

The user interface is organized with the help of docking windows. The following figure shows them at a glance.

Part view

Part view

  1. Table (the loaded part's standard name is displayed on the tab)

    There are two sub-dockings which represent two different modes to determine the characteristic.

  2. Links to similar objects (see Section 3.1.7.4, “ Docking window "Links" ”)

  3. Assembly / Bill of material (see Section 3.1.7.5, “ Docking window "Assembly" ”)

  4. 3D preview of the object (see Section 3.1.7.6, “ Docking window "3D view" ”)

  5. Technical details with dimensioning views (see Section 3.1.7.7, “ Docking window "Technical details" ”)

  6. Part information (see Section 3.1.7.8, “Docking window "Part information" ”)

  7. Topology information (see Section 3.1.7.9, “Docking window "Topology information "”)

Optionally, other dockings are displayed: