Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following describes how you can insert single 3D parts from the Standard and supplier parts library into your 3D CAD system.
Note | |
---|---|
This is the description of the default procedure. For some CAD systems you can find further information in the CAD specific chapter. |
In the Part selection choose the desired parts.[10]
Determine the desired characteristic in the Part view.
Click on .[11]-> The display returns to the CAD system.
If you performed a search, you can directly export from the search results.
In the CAD system, the PARTsolutions placement dialog appears.
|
The placement methods available in particular depend on the part type.
Not all parts in the standard catalog have all the attributes needed for additional PARTsolutions intelligent placement methods. The method "Default placement" is always available. Currently the CAD interfaces enable the additional intelligent placement methods for rotationally symmetric parts such as bolts, nuts, rings and bearings for example.
The following figure gives an overview about the parts which enable intelligent placement in addition.
-> Now in the placement dialog the following buttons are shown.
Place multiple (and leave dialog opened) | |
Place once (and close dialog) | |
Close dialog box (without placement) |
The activation of the Repeating checkbox enables the repeated placement in the CAD without having to use the [12] button.
[10] A detailed description of PARTdataManager can be found under Section 3.1, “ PARTdataManager ”.
[11] You can also export the part via "Export in file". More detailed information can be found under Section 3.1.9, “ Export into different file formats (without PARTsolutions interface) ”.
[12] At certain CAD systems the function is available for all placement methods, at others only for the Standard CAD placement method. If the function is not available, then the checkbox is grayed out.