Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The part selection follows the following steps:
Determine the characteristic via row selection at the desired CAD model |
||
|
|
|
Follow the steps listed below to reach your desired part:
Select the desired catalog or directory.[130]
After you have selected a catalog, you can select the catalog language in the navigation path (if several catalogs are available, otherwise at once).
Select product
groups as long as a concrete assembly or concrete single part
has been specified.
Choose an assembly or a single part.
As soon as a concrete row has been determined, you can load a 3D view and dimensioning views (if available) under CAD model preview. Therefor, click on the button .[131]
-> Part is loaded under CAD model preview.
Define the characteristic of the part by clicking into the option button (at the left on the desired row).
Variable view (possibly set value ranges). Details under Section 4.5.1.3, “How can I adjust the value range fields in the variable view?”.)
In order to reach the variable view, click on the part link or preview image.
-> Now you can see all variables in list form.
In case value range fields are available, you will recognize this by the yellow-highlighted fields and on the right side by the table symbol.
Click on
Back
to get to the table again.
[130] The exact depiction differs depending on portal. On the level of Home directory you can see the subdirectories of the root directory. (If there is only one catalog available, you can see part folders. If there are several catalogs available, these are shown in the first step.)
[131] Of course you can specify a concrete characteristic first and then generate the preview.