Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The direct integration (PART2cad) simplifies the download of CAD models. These are loaded quickly and directly into the CAD system. Temporarily saving of parts is not necessary.
Proceed as follows to directly integrate the selected CAD model into your CAD system:
Make sure that the desired part is specified in the table view (and in the variable view if there are value range fields).
-> The format selection dialog opens. At the desired one, activate the checkbox. (Only one selection is possible.)
-> The desired component is generated und displayed below ready for download.
-> The direct integration is starting.
Install it during the first run. The necessary installer opens automatically.
The installer itself needs Java.
-> Once Java is installed the PART2cad installation will start. If Java is not installed, there will be no Java logo displayed. In this case click on the link and install Java.
-> Warning messages may show up. Allow the installation of the component PART2cad.
During the first run the direct integration PART2cad will be downloaded.
Following runs will open the dialog Transferring model to CAD. No user interaction is necessary.
In the drop-down menu select the CAD version where the model is to be transferred. Confirm the selection with .
-> A specific dialog box according to the used CAD system is displayed. Perform the required settings.
Select the preferred destination directory. Use to browse. Confirm your entries by clicking .
-> The model is transferred to the CAD system.
-> The part has been imported into the CAD system.
If the CAD system is not started or the wrong version was chosen, an error message will be shown.